Power Rail and Lines
- The power rail on the left represents the TRUE value and initiates the
rung state.
- Any object connected to this rail is always powered.
- Horizontal lines always represent a data flow from the left to the right.
- If a vertical line has several items connected on the left, then it represents an OR / ORN operation.
- You can insert a segment of horizontal line at any location to freely draw flow lines.
- The vertical line button is used to set or remove (toggle) a segment of vertical line on the right of the selected cell.